This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ACT14: Parallel use of two IC packages.

Part Number: SN74ACT14
Other Parts Discussed in Thread: UCC27517, UCC27518

Hi team.

We want to output an 8.2MHz singnal from SN74ACT14PWR by using two IC packages.

Use by connecting 3Y, 4Y, 5Y, 6Y pins of each IC at one point.

The VCC is 5V, and all the output current is assumed to be 260mA.

Is there a risk that the IC will be damaged by connecting the output pins?

Best regards.