Other Parts Discussed in Thread: SN74LVC244A-Q1
Hi,
my customer use txs0108eqpwrq1 in orin platform, port a 1.8V, port b 1.8V,
A port input 0v, B port output 0.45V, that over spec, should low than 0.4V. that is tow chip parallel result in?
B port input 0V, A port output 0.2V.
the Processor request low voltage should <0.4V.
How to let the output low than 0.4V? can I add 10K pull down resistor?
Best regards,
jeff wang