Other Parts Discussed in Thread: SN74AHCT1G125, SN74AHCT1G126, SN74LVC1G99, SN74LXC1T45
Hi guys,
As suggested on this thread by TI engineers: https://e2e.ti.com/support/logic-group/logic/f/logic-forum/887817/txb0104-trying-to-adapt-voltage-levels-for-an-sdi-12-bus-with-a-3-3v-mcu
to use a combination of SN74AHCT1G125 + SN74LVC1G17 to implement the voltage translation from SDI-12 bus to 3.3V MCU.
But, with the present of the SN74LVC1G17 which shared a single pin used both TX and RX mode, the output of the SN74AHCT1G125 will not work (goes flat). When toggling the pin (IO33 in schematic) at 3.3V, the measured input of SN74AHCT1G125 about 0.5V only and output of SDI bus voltage level (output of SN74AHCT1G125) is 0V. If I were to remove the SN74LVC1G17 chip, then the SDI bus voltage level (output of SN74AHCT1G125) goes to 5.0V as expected. And input of SN74AHCT1G125 goes to 3.3V as expected driven by the MCU.
This is how the connection looks like: