Part Number: SN74LVC1G08-Q1
Hello TI team,
please help to check the CTE information. thanks.
| Part CTE | PCB CTE | ||
| SN74LVC1G08QDCKRQ1 | X | Y | Z |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC1G08-Q1
Hello TI team,
please help to check the CTE information. thanks.
| Part CTE | PCB CTE | ||
| SN74LVC1G08QDCKRQ1 | X | Y | Z |
Hi Amy,
For precise information, an NDA is required which you would work with your local TI sales office to arrange. The TI FAE can contact me regarding specific details in a non-public forum.
If you just need general values of CTE for components of the device, then I can provide those here:
Copper (primary metal for lead-frame construction) ~17 ppm/⁰C
NiPdAu coating (outer layer of leadframe) ~13 ppm/⁰C
Sn coating (alternate outer layer of leadframe) ~21.5 ppm/⁰C
Mold compound (plastic body) ~12 ppm/⁰C
Silicon ~2.6 ppm/⁰C