This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G08-Q1: Part CTE and PCB CTE

Part Number: SN74LVC1G08-Q1

Hello TI team,

please help to check the CTE information. thanks.

Part CTE PCB CTE
SN74LVC1G08QDCKRQ1 X Y Z
       
  • Hi Amy,

    For precise information, an NDA is required which you would work with your local TI sales office to arrange. The TI FAE can contact me regarding specific details in a non-public forum.

    If you just need general values of CTE for components of the device, then I can provide those here:

    Copper (primary metal for lead-frame construction) ~17 ppm/⁰C

    NiPdAu coating (outer layer of leadframe) ~13 ppm/⁰C

    Sn coating (alternate outer layer of leadframe) ~21.5 ppm/⁰C

    Mold compound (plastic body) ~12 ppm/⁰C

    Silicon ~2.6 ppm/⁰C