This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AVC32T245: High Density Voltage Translator

Part Number: SN74AVC32T245

Hey team,

What parts would we recommend for high density voltage translators? A customer is trying to translate 100-130 signals so would prefer >8 bit solutions.

They are translating from 1.1V to 3.3V and would be translating signals from DC to 50MHz (in general).

I initially thought the SN74AVC32T245 would be a good fit, but I realize that if the supply rail is 3.3, that limits the minimum voltage the device can accept as a 'High', right?

Thanks,

Cameron