Hi,Johnny
我们的应用场景如下,

测试到的波形如下:
蓝色为A-PORT输入,黄色为B-PORT输出
理论上黄色波形应为高电平3.3V的方波,但实测高电平为2.5V左右,上升沿有瞬间冲到3.3V左右然后回落2.5V;
请帮忙确认下为何会出现这种情况?这种情况是否正常?谢谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,Johnny
我们的应用场景如下,

测试到的波形如下:
蓝色为A-PORT输入,黄色为B-PORT输出
理论上黄色波形应为高电平3.3V的方波,但实测高电平为2.5V左右,上升沿有瞬间冲到3.3V左右然后回落2.5V;
请帮忙确认下为何会出现这种情况?这种情况是否正常?谢谢!

Your actual circuit has a load that is not shown in the schematic. The edge accelerators of the TXS work only for a few nanoseconds; after that, the voltage is held high only by the internal 4 kΩ pull-up resistor. So I guess you have a pull-down resistor with about 12.5 kΩ, or a current sink with about 200 µA.
Hey Zhiheng,
Welcome to E2E forums! It is strongly recommended to remove the pull down resistors as TXS family devices have internal pull up resistors. Combining these two elements will create a voltage divider and cause a decrease in VOH levels. See this app note for more information.
Regards,
Jack