Part Number: SN74LVC541A
One of our programs is using this part at 3.3V and started seeing part failures. When they replace this component, the board works again.
We sent the failing parts, and new-from-stock parts to our lab for testing.
The lab used 3.6V supply. All VoH, VoL, and input current tests passed just fine, but the parts fail AC testing.
The lab ran H->L, L->H, Enable, and Disable tests at room temperature with no load on the outputs.
They measured anywhere from 12.6 to 26.6 ns delay time. The datasheet says the limit is 5-7ns. Here's the results from one part:
AC Test AC3THL: *Failed @ 18.1ns (Range 60.0 to 4.0 - HiLimit: 5ns)
AC Test AC3TLH: *Failed @ 17.9ns (Range 60.0 to 4.0 - HiLimit: 5ns)
AC Test AC3OEN: *Failed @ 12.6ns (Range 60.0 to 4.0 - HiLimit: 7ns)
AC Test AC3Tdis: *Failed @ 26.4ns (Range 60.0 to 4.0 - HiLimit: 7ns)
We've seen 2-4 ns difference in times on similar tests due to the tester, but that doesn't account for these results. I'm including a couple of the scope traces.
Ch1 input, Ch2 output, Ch4 is a trigger used to select a random signal from within a repeating test, so we're not picking up the very first result.
Can you offer any suggestions as to why we're seeing such slow propagation times?
e have 44 digital signals ( all in +3.3V level ) connecting to the input of LVC541A buffers. All these inputs would be having either of both options below (either 158K pull up or 158K pulldown resistors). There are external clamping diode used in the schematic for any of the signals.