Other Parts Discussed in Thread: SN74AXCH4T245
Guys, does TI have the min and max data of tPLH, tPHL base on SN74AVCH4T245 1.2 to 3.3V? Datasheet just show the typ. data as below picture.
Thanks in advance!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Guys, does TI have the min and max data of tPLH, tPHL base on SN74AVCH4T245 1.2 to 3.3V? Datasheet just show the typ. data as below picture.
Thanks in advance!
1.2 V is the lower limit of the supply voltage; 1.199 V is not guaranteed to work. So you are not supposed to use a nominal 1.2 V supply with this device.
Use the SN74AXCH4T245 instead.