Hi,
On data sheet, 10ns/V is max. SR at 1.8V. So the rising / rising time will be 10*1.8 = 18ns, right? In other words, the max. freq. is 1/36ns = 27.78MHz only at 1.8V. Is it correct?
Is there part suggestion for 125MHz/ 1.8V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
On data sheet, 10ns/V is max. SR at 1.8V. So the rising / rising time will be 10*1.8 = 18ns, right? In other words, the max. freq. is 1/36ns = 27.78MHz only at 1.8V. Is it correct?
Is there part suggestion for 125MHz/ 1.8V?
Hi Alan
To clarify Clemens Δt/Δv is used to refer to how slow your rising edge is allowed to be before you might have issues relating to a slow input signal. You are meant to operate under this maximum time.
With a 15 pF load, the maximum propagation delay is 1.5 ns, which corresponds to 333 Mhz.
This device I is officially rated to 275 MHz (Looking at SN74AUC1G74), but given it's not a clocked device it's actual max could be closer to what Clemens put.
Regards,
Owen
Hi Owen,
the rising/ falling time is 0.75ns max. at 1.8V. so looks like no issue at 125MHz with 1.8Vcc, right?