If VCC is 0VDC, and the inputs to the SN74LV244AT are beginning driven to a TTL high from another active TTL device will the powered off SN74LV244AT input clamp diodes pull DC current and backflow to the VCC of the no powered SN74LV244AT?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If VCC is 0VDC, and the inputs to the SN74LV244AT are beginning driven to a TTL high from another active TTL device will the powered off SN74LV244AT input clamp diodes pull DC current and backflow to the VCC of the no powered SN74LV244AT?
Hi Michael,

Per the datasheet, the inputs will be high impedance when VCC = 0V, with a maximum leakage of 5uA across process and temperature variations.
For more info on how to identify if a device has a positive clamp diode or not, please see: [FAQ] Can the input voltage (Vi) to my logic device be higher than the supply voltage (Vcc)?
We also have some more info on the "Ioff" feature here: [FAQ] What does 'partial power down' or 'Ioff' mean in the datasheet?
Please let me know if I can be of further assistance.
Hey Michael,
No problem - we generally get back to people on the same day, although it is common to see delays over holidays / weekends. Come back any time!