Hello,
My customer would like to achieve hot-swap level-1 at their application.
This means that they can accept data corruptions during hot-insertion/removal, but can not accept device damages.
My customer has some questions as follows.
Q1:
My customer thinks SN74AVC4T245 is hot-swap level-1 device. Though the following app note states a “the host system must suspend signaling during daughter-card insertion or removal at level-1 isolation, does host really have to suspend signaling during the insertion or removal to prevent device damages? How SN74AVC4T245 could be damaged if the host system does not suspend the signaling during the insertion or removal? https://www.ti.com/lit/an/scea026/scea026.pdf?ts=1672555633359
Q2:
When SN74AVC4T245 is used at host side, not daughter card side inserted or removed, are there anything customers should care about?
Best regards,