Other Parts Discussed in Thread: SN74HCS244-Q1
For dual Buffer part no. SN74LVC2G17QDCKRQ1, input voltage Vin of 5.5V can be applied, even if VCC is 3.3V, right? Or will Vin_max be 3.3V (same as VCC) only?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For dual Buffer part no. SN74LVC2G17QDCKRQ1, input voltage Vin of 5.5V can be applied, even if VCC is 3.3V, right? Or will Vin_max be 3.3V (same as VCC) only?
Hello,
For dual Buffer part no. SN74LVC2G17QDCKRQ1, input voltage Vin of 5.5V can be applied, even if VCC is 3.3V, right?
Yes, that is correct.
Or will Vin_max be 3.3V (same as VCC)
Our datasheets will indicate VCC as the maximum if that is the case. You can see an example with the SN74HCS244-Q1. SN74HCS244-Q1 Recommended Operating Conditions