Other Parts Discussed in Thread: SN74LVC2G66, TS5A2066
We have used the SN74LVC2G34 dual buffer gate in our circuit which is used to drive an AND gate which inurn controls a regulator that powers on the device.
the pins given to the SN74LVC2G34 dual buffer gate are being driven high from the MCU side so as to power on the regulator. voltage of the 2 lines are 3.3v but after the buffer implementation the voltage at these lines drop to 0.56V ,whereas we expect it to be around 3.3V.
when we connect it directly without the buffer circuit we see that there is no issue.
could you please confirm what is causing this drop.
also wanted to know the working of the SN74LVC2G34 dual buffer gate during initial condition (during first time power up)
please find the image of the circuit implementation attached and share your feedback..
regards,
Aagneya C