This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G126: Output of 1G126 when the OE is 0.8V

Part Number: SN74LVC1G126
Other Parts Discussed in Thread: TPS3897, UCC27516, UCC27517

Hello

I would like to understand the power up status of 1G126. I use the TPS3897 output to control the OE of 1G126.

During the power up process, the output of TPS3897 could be 0.8V if the supply voltage of TPS3897 does not reach 0.8V.

So the question is, if the OE of 1G126 is 0.8V, and the supply voltage is also 0.8V, will 1G126 output a 0.8V despite of input voltage.