I observe some anomalies in the datasheets of AUP1G80, AUP1G79, AUP2G80, AUP2G79, AUC1G79, AUC2G79.
Let's look at 1G80:
a. There is a fclock in chap. 6.7 and there are fmax values in chap. 6.8-11. It is unclear what their relationship is.
b. It is somewhat surprising that fmax at higher supply voltages does not increase as the capacitive load is reduced.
c. In many cases the typical fmax value at 25°C is lower than the min. fmax over the temperature range.
This cannot be, no way!
One would expect the typical value to be at least twice the worst case value, the small magin, where it is, IMHO is technically implausible.
The same applies to the AUP2G80 and AUP2G79 datasheets.
d. In the AUP1G79 datasheet in chap. 6.6 and 6.8 the frequency is given in ns, should be MHz, of course.
Same for the AUC1G79 datasheet. Same for the 30pF values in AUC2G79. Same for the 30pF values in AUC1G80 and AUC2G80. Same for the 30pF values in AUC1G74.
(Nine buggy datasheets makes a sixpack of beer for me, right?)
I am particularly looking for a (ripple) frequency divider with AUP2G80 or AUC2G80 i.e. cload <5pF.
I guess the chip is much better than the datasheet says (... compare competitor!)