Other Parts Discussed in Thread: SN74LVC1G125-Q1, SN74LVC1G126-Q1, SN74LVC1G99-Q1, SN74HCS21
Hi Expert,
I'm verifying the "AND" logic IC SN74HCS21-Q1 for our project. I found an abnormal phenomenon from this chipset. Showing the waveform below.
In it, the DSP_RST is from the output of the IC. UG1V_PG and MCU_PA15 is the input of the IC. UG3V3 is the VCC of the IC.
We can see that the output will have a glitch when VCC is rising up, even though the one of the input is low. In the time. We expect the output should be low without glitch.
Do you know this issue? And how can we avoid this glitch appearing? Or any other IC with the same function to recommend to us?
Thank you,
Best regards,
Haiming.Qu