Hi TI,
Q1. In case of PCIe EP mode Vref_B:VPH_PWR(3.3V), it would be 3.3V -> 1.8V. (Down translating)
Then, If PCIE_RST_N has no pull-up, PCIE_RST_N's voltage is 1.8V?
I'm wondering that in this case 1.8V will be the threshold value that controls the LSF device for all channels.
Because LSF's FET is Hi-Z status when Vref_B is high.
Is what I have understood correct?
Q2. Is it okay to apply 100 K pull-up for Vref_B line?
Thank you.
Best Regards,
Seunghwan Lee.