Part Number: SN74LVC1G97-Q1
Hello,
SN74LVC1G97-Q1 can be used with supply voltages between 1.65 and 5.5V and the input voltage rating specifies that the abs max is 6.5V. If the device VCC is powered at 3.3V (to be compatible with 3.3V logic), are the pins still 5V-tolerant? I understand that the input thresholds are related to VCC, but I want to confirm that the input voltage rating is not.
Thanks,
Nicole