This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G07: Design | SN74LVC1G07 | VLoad

Part Number: SN74LVC1G07


Hi Team,

1. Could please explain what is Vload? How it becomes 2*VCC?

2. In our design we are using VCC as 5V. Since RL is 500ohm. Will it work if we give 10K pull up in the input?

    Vinput = 5x(500/1500) = 1.6V <3.5V