This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0106: Device malfunction, maybe related to OE pin

Part Number: TXB0106
Other Parts Discussed in Thread: TXU0304, TXU0202, TXU0101, SN74LVC125A, SN74AXC4T245, SN74LVC2G34

Hello,

I'm trying to interface a modem (uBlox SARA 422S) to an ATmega1284P through a SPI/RS232 transceiver (PI7C9X760).

1.8V (line 1V8) is provided by modem when it is running (PWR_SW pull down and RESET done). Modem uses 1.8V logic. Thus PI7 is powered by 1V8 line.

TXB0106 is between processor and SPI/RS232 bridge as it provided isolation between SPI bus and PI7 bus.

In this configuration, TXB0106 doesn't run as expected. I have read again datasheet and I have seen that OE should be tied to VCCA after VCCA and VCCB are stable. Is a simple reset circuit (RC) enough to generate OE signal ? For example this kind of reset:

And can TXB0106 run in this configuration?

Best regards,

JB