This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHCT1G08: Difference between SN74AHCT1G08DCKR(E) and SN74AHCT1G08DCKR

Part Number: SN74AHCT1G08

Hi Team

Could you please tell me the difference between SN74AHCT1G08DCKR(E) and SN74AHCT1G08DCKR?

Best regards,

Kenta

  • The difference is that "SN74AHCT1G08DCKR(E)" is not a valid OPN.

    I suspect that a customer added this suffix to indicate that both SN74AHCT1G08DCKR and SN74AHCT1G08DCKRE4 are allowed.

    (If you're asking about C0JBAA000419: it is used only as a 3.3 V to 5 V level shifter, so the SN74AHCT1G08DCKR will certainly work.)