This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0104E: Is A side 10Kohm pullup active with VccA = 1.8V and VccB = 0V (unpowered)

Part Number: TXS0104E

Hi,

with VccA powered and VccB unpowered, is the internal 10Kohm pullup active on the A side.

The OE is pulled to A side 1.8V.

We turn ON VccB at a later time after startup.  Before turning ON VccB we do i2c transactions and our risetime are very slow and do not correspond to a typical 10Kohm pullup. Unless there is added capacitance on the A side I/O pin with B side unpowered.