Other Parts Discussed in Thread: SN74LVC1G32-Q1
Hello, please ask if the SN74LVC1G97QDCKRQ1 can be replaced by a two-input or gate logic IC, and is there a recommended model
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, please ask if the SN74LVC1G97QDCKRQ1 can be replaced by a two-input or gate logic IC, and is there a recommended model
It can be replaced by the respective SN74LVC1Gxx AND/OR/buffer/inverter gate, depending on how it is configured.
This picture comes from TDA4 EVM reference design,so my question is : can U279 ( in the red circle) be replaced by a common 2 input AND/OR gate IC. please give me a detailed part number
U279 is configured as an OR gate. The SN74LVC1G32-Q1 would have the same function, but has a different pinout and has no Schmitt-trigger inputs.