Part Number: TXU0304
Hi, we plan to take a 24MHz signal into three of the inputs of the TXU0304. The input and output will be supplied with 1.8V thus no level translation will occur. The three outputs will be going into loads with a maximum jitter spec of 70ps. Assuming the source 24MHz has no jitter, how much jitter would the TXU0304 add?
Going off the propagation delay tables in the datasheet, if the delay has a minimum of 0.5ns to 22ns, this variance could attribute to 21.5ns jitter correct?