This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1T34: SN74AUP1T34DCK_Clarification on voltage levels

Part Number: SN74AUP1T34

HI,

I'm using SN74AUP1T34DCK as unidirectional level translator for the RESET signal which is shown in below schematic screenshot.

I would like to just confirm that here I have given 3.3V to VCCA and 1.8V to VCCB, is that OK? since VCCA and VCCB are supporting 0.9V to 3.6V and there is no voltage level condition like VCCA<=VCCB in the datasheet.

Regards,

Chitharanjan M