This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN54LVTH162244-SP: space part vs military rated version

Part Number: SN54LVTH162244-SP
Other Parts Discussed in Thread: SN54LVTH162244

Hello,

Quick question about SN54LVTH162244-SP. Is this part built any differently than the Military rated version, SNJ54LVTH162244WD, or just qualified to a different level? What would the orderable device look like for the space rated part (SNJ54LVTH162244WD-SP or something else?)

Thanks,
Adam

  • 5962-9680901QXA: SN54LVTH162244
    5962-9680901VXA: SN54LVTH162244-SP

    Both use the same SMD. The letter Q/V is the device class designator (high reliability/space, see section 1.2.3). Section 4.2.1 c. says that "additional screening for device class V beyond the requirements of device class Q shall be as specified in MIL-PRF-38535, appendix B." Section 4.4.1 d. table II lists the different electrical test requirements.

    The material content is identical down to the last digit, so it appears to be the same.