This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1T32: Output state with an Open Input.

Part Number: SN74AUP1T32


If either input A or B, pins 1 and 2 respectively, are left open can the input be considered a logic 0 at that input.  In other words, if A input is low at 0V and B is left open can I be sure the output will go to logic low(0Volts)?