Other Parts Discussed in Thread: SN74AXC4T774
I'm looking into use the TXU0304 in an SPI application converting from 1.8V to 2.5-3.3V. Speed of SCK is 32MHz. At a first glance the TXU0304 should be suitable, but when investigating the propagation delay one can see that it's broadly specified 0.5-20ns (approx). With worst case 20ns there will be a time-difference between SCK and MISO (slave-out) of more than 40ns at the master (2*propagation delay in TXU0304 + set-up time for slave) and therefore you cannot use the TXU0304 for such high speeds?!
Do you have any solution or suggestion for solving this?