This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN54AHC244: when max 2.5V control state, is it correct operating? (VCC 3.3V)

Part Number: SN54AHC244

Dear High Reliability team.

The below is datasheet for the part.

Can I apply 2.5 V(max) for Vih pin (when sn54ahc244 VCC is 3.3V)? Doesn't this cause operating problems?

unfortunately, My output voltage of controller IO is max 2.5V.

In range whole of operating temperature, Is it possible?

thankyou