Other Parts Discussed in Thread: SN74AUC244, SN74LV244A, SN74LVC244A, SN74LVC541A
Tool/software:
Hi,
I'm using the buffer SN74ALVC244 to drive some other IC input pins on an existing PCB.
The IC is already active before the buffer Vcc is on.
The IC pins can't be left floating. The IC can be configured to have internal PU resistor (not PD).
Can I connect the internal PU to the buffer's output when the buffer is off?
According to the buffer's datasheet, the output voltage range is VCC + 0.5, but it "may be exceeded if the input and output current ratings are observed."
I am not sure if the buffer has a clamping diode only to GND or also to VCC? The condition for output clamp current is "Vo<0".
Is there a more suitable buffer for this case, with the same specs? (same Tpd, footprint)
Thanks