This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0104E: Can I use the TXS0104E as a replacement for the TXS0102 for I2C applications?

Part Number: TXS0104E
Other Parts Discussed in Thread: TXS0102, TXB0104, , TCA9800, TCA9803

Tool/software:

Hello,

I have some questions regarding your voltage translators.

According to the information displayed beneath the featured voltage translators image, it appears that only the TXS0102 is recommended for I2C, while the TXS0104 is indicated for I2S.

In this context, I'd like to inquire whether it's permissible to use the TXS0104 for I2C applications. Additionally, if I2C compatibility is confirmed, I'd like to know if there are any issues associated with exclusively using the TXS0104 for I2C communication.

I have an additional question regarding your voltage translators.

The image does not indicate GPIO functionality for the TXB0104 and TXS0102. I would like to inquire whether it's permissible to use these devices for GPIO purposes.

Regarding the TXB010X Series and TXS010X Series, I'd like to inquire whether the difference in the last digit primarily indicates the number of bits or if it signifies a difference in purpose.

Additionally, I'm experiencing signal degradation when using TXS0104 and TXS0102 consecutively on the board, as shown in the circuit diagram below. I'm inquiring about possible solutions to ensure signal integrity.

Thank you.

url :  translators & level shifters | TI.com