Part Number: SN74LVCC3245A
Tool/software:
I have a guess on the max capacitive load this your chip is validated to use but it isn't clean on the data sheet and seems low to me.
We have circuit:

The processor pushes OUT1_3.3 on the A7 input controlling the B7 output. Part U19 has 10pF cap and I'm not worried about that. This issue is we want to change R226 to a capacitor, but there is not a clear max output capacitance that I saw on your data sheet that the U16 (SN74LVCC3245A) can push.
Can you clearly say what the typical and max output that your chip can push that I should validate the system with?
Thanks
Nick
EE