Tool/software:
Hello.
What is the maximum input voltage for input terminals such as SER and OE?
In the Input clamp current item, it says Vi>VCC+0.5V, but is the idea that VCC (Max) 7V+0.5V=7.5V correct?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello.
What is the maximum input voltage for input terminals such as SER and OE?
In the Input clamp current item, it says Vi>VCC+0.5V, but is the idea that VCC (Max) 7V+0.5V=7.5V correct?
The limit always depends on the actual supply voltage.
In practice, the supply voltage will not be 7 V, so in practice, that 7.5 V value does not matter.
The recommended operating conditions do not allow voltages above VCC. What is the actual problem you're trying to solve?
Thank you for your reply.
What I want to know is the absolute maximum rating of the input terminal.
I would like to know the permissible value because the voltage at the input terminal can be higher than VCC.
There are clamping diodes to VCC; see [FAQ] Can the input voltage (Vi) to my logic device be higher than the supply voltage (Vcc)?
When you limit the current to something near zero, the forward voltage will no more than 0.5 V (so VCC + 0.5 V is always safe). But for larger currents up to 20 mA, the forward voltage will be higher.