Part Number: SN74LVC1G00
Tool/software:
Hi Team,
What is the VOH and VOL levels when VDD=3.3V and VDD=5V??
There is no detail given in datasheet.
Regards,
Vidhya
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74LVC1G00
Tool/software:
Hi Team,
What is the VOH and VOL levels when VDD=3.3V and VDD=5V??
There is no detail given in datasheet.
Regards,
Vidhya
Use the values specified for 3 V and 4.5 V; those are the worst case of 3.3 V ± 0.3 V or 5 V ± 0.5 V supplies.
Hi Vidhya,
-Owen
HI Owen,
Interpolation is not clear in excel. What are the limits for 3.3V and 5V VDD?

min and max, m levels in equation.
Thanks,
Vidhya
The min and max levels would be the known datasheet values. For 3.3 V VOH Xmin is 3V X max is 4.5V Ymin is 2.3 and Y max is 3.8
-Owen