This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVCC3245A: Regarding abs for Iout

Part Number: SN74LVCC3245A

Tool/software:

Hi support team all.

I have a question about the following two devices.

-SN74LVCC3245APWR

SN74LV541APWR

Q1:

The absolute maximum ratings for the output current Io is

SN74LVCC3245APWR: ±50mA

SN74LV541APWR: ±35mA

Do both of the above apply to only one output or to the total of all eight outputs?

Q2:

For example, regarding the SN74LVCC3245APWR

the high level output current (IOHA) is listed as -24mA (VCCA: 2.7V/VCCB: 5.5V),Does this value apply to 1 output or total of all 8 outputs?

Also, is it possible for all outputs to be -24mA at the same time (all pins B1 to B8)?

Best regards,

Higa