This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G07: Buffer connection to separate two different voltage level

Part Number: SN74LVC1G07


Tool/software:

Hello,

I have attached the connection diagram of my SN74LVC1G07 that we have done in our project.

The thing is that the Input of the Buffer (that is our microprocessor's output pin and it is logic is CMOS, 1.8V)  is 1.8V and the output is 3.3V. The microprocessor pin will control the output. Actually the other option is there level shifter but we don't want to use it because the voltage level of M2E_SUSCLK_32KHZ may vary between 1.8v & 3.3V. 

so can we use SN74LVC1G07 like this to fulfill our requirement, if not could you suggest any other possible solution.

Best regards,

Eva