Part Number: SN74LVC1G175-EP
Tool/software:
Hello support team,
I am using D flip flop with part number: CLVC1G175MDCKREP.
- My problem: The Q output doesn't go high.
- Description: On the circuit I am soldering R244 = 20K, C383 = 22uF, D27 not fitted. The #CLR signal reaches a high level, after about 4.3 seconds CLK changes from Low to High. However, the Q pin still remains low.
- I have soldered a push button in parallel with C383, if I press it then Q goes high.
Please let me know the problem and solution.
Thanks for supporting me,
Regards!
,