This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ALVC04: Propagation delay and drive strength

Part Number: SN74ALVC04


Tool/software:

For the SN74ALVC04:

  1. Is the propagation delay from input to output the same when input goes from "H" to "L" as when input goes from "L" to "H" ?
  2. Can you connect outputs from the same device like below to improve the drive with out destroying or reducing life of the device?

Thanks.