Tool/software:
Hi team,
Can the TPLD1201 be used as a level shifter to input 1.8V logic levels and output 3.3V when supplied with 5V Vcc?
Best regards,
Kyohei
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kyohei,
This is possible if the customer uses input pins configured as low-voltage digital inputs and output pins configured as open drain outputs, with external pull-ups to 3.3V (not using any internal pull-up resistor).
Best,
Malcolm