This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC573A-Q1: Should LE be pulled down?

Part Number: SN74LVC573A-Q1


Tool/software:

Hi, I'm trying to determine if LE needs to be pulled down in my design.  The plan is to have OE pulled high on the board and then drive it low once power has reached a steady state, LE will also be driven low at this time.  The latches will then remain inactive until there is a command to send input values and latch them.  All of the inputs will be pulled down.  So my question is, should LE be pulled down as well?  Obviously when the inputs are ready to be latched LE will be pulsed high.  I'm just trying to determine if I need to pull LE low on the board or if driving it low after power up is sufficient.