Tool/software:
Hi,
We are currently experiencing an issue where the +3.3V system is being damaged in a circuit utilizing the TXS0108E.
We would like to understand the possible causes and countermeasures for this issue, and we would appreciate your guidance on the matter.
■ Circuit Configuration
In our design, we are using the TXS0108E with the following setup:
- VCCA side (3.3V system): Push-pull I/O
- VCCB side (5V system): Push-pull I/O
- Bidirectional communication via TXS0108E
■ Issue Encountered
- The +3.3V system is being damaged at an unknown timing, and this has occurred multiple times.
- We would like to confirm with TI whether any of the following conditions could lead to such damage:
- If VCCA is powered, and a negative voltage (0V or below) is applied to the VCCB side, is there a possibility that current could pass through TXS0108E's internal resistors (R1/R2) and cause stress on the VCCA side?
- Under certain conditions, could a 5V signal from the VCCB side be directly transferred to the VCCA side, causing unexpected voltage levels?
- Are there any other precautions regarding the use of peripheral components that could lead to excessive load or damage to TXS0108E or the +3.3V system?
We have reviewed the datasheet specifications, but we would like to receive an official response from the manufacturer regarding these concerns.
Thanks,
Conor