This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0104E: The parameter problem of the chip

Part Number: TXS0104E

Tool/software:

How much current is required for the VCCA and VCCB of the material TXS0104EPWR? We have a circuit output of only 150mA and we want to use this material to convert 4 GPIOs.

Our internal power supply is very small, if 100mA May be risky

Please confirm the TXS0104EPWR chip power supply current

If it is  to be 100 ma, but this positive or negative I understand is that the GPIO of A communicating with B's gpio has a lower GPIO current of 100 ma.

Please help to confirm the chip power supply current of VCCA and VCCB of TXS0104EPWR again. Is this current pulled from GPIO?And the value of this current, what are the typical values and the maximum values?