Other Parts Discussed in Thread: SN74HCS04, SN74LV14A, SN74LVC14A
Tool/software:
Dear TI experts, as it stands now, I currently have no trust in SPICE models provided for TI parts. Please can you elaborate on the following:
1) The SPICE model on this page: https://www.ti.com/product/SN74AHC14#design-tools-simulation has this on line 118 in SN74AHC14.cir:
.PARAM MAXICC = maxICC
which brakes the model since maxICC is just a spaceholder.
2) SPICE models for other candidate devices I am trying to compare it against have the following equivalent lines:
SN74HCS04.cir (line 118): .PARAM MAXICC = 0.0009
SN74LV14A.cir (line 118): .PARAM MAXICC = 0.032
SN74LVC14A.cir (line 124): .PARAM MAXICC = 0.032
which makes the models not broken but also not exactly credible. Datasheets are not unified in what parameters they convey and how, so they do not provide the basis for direct comparison between those parts.
Therefore, I am trying to simulate the shoot-through current during a switching event triggered by a slow input. I get some nonsensical values. Powered by 3.3 V, I get peak currents of 1.54 mA (which actually seems about right), but also 37.6 mA and 51.4 mA (on the rising output edge) for those three devices, U1, U3 and U4 respectively (U2 is AHC and is excluded since it brakes the simulation):

The whole point of trying to simulate it is to be able to identify a device which will consume the least amount of power in my particular application scenario, both statically and during switching events. However, I cannot simulate the AHC device at all because of its broken model, while the results from the other three models do not instill confidence.
Can you please fix these models so they would be accurate at least relative to each other? Thank you so very much! Best regards,
Marko Dukši