This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0108-Q1: Bi-directional step-up not working LSF0108-Q1

Part Number: LSF0108-Q1


Tool/software:

I am trying to step up, and stepdown SPI through this LVL shifter. I would like to go from 1.8V to 2.5V, and back down again. I cannot seem to get the step-up functionality to work. 

Even on a test setup, where only GND, VREFA, VREFB, and enable are selected, if I put a clock signal at 1.8 in, it STAYS 1.8 on the output. However, IF I switch to the B side with a 2.5 signal, it does get reduced to a 1.8.

The chip mentions auto-bidirectional, is there something that I am missing?

I know there needs to be a .8V increase between the references, I have tried 1.8 to 3.3 and still no luck