Part Number: SN74LVC1G79
Other Parts Discussed in Thread: SN74LVC1G374
Tool/software:
Hi team,
My customer is using SN74LVC1G79 and met issue during the power on.

Magenta channel 4 is the D input signal of the trigger, yellow channel 1 is the 5V power supply, green channel 2 is the clk signal, and blue channel 3 is the output of the trigger; the current phenomenon is that when the D input and clk signal of the trigger are both low, the output of the trigger will follow the 5V power supply voltage, and the duration is 7.44ms.
Q1: Is it normal during the power on and output automatically sets to high.
Q2: Can SN74LVC1G374 be used for solving this issue? We want to keep OE high when power on and set it to low after power on.

Q3: Do we have relevant device with opposite OEn logic vs SN74LVC1G374?