This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G123: Pulse duration time

Part Number: SN74LVC1G123
Other Parts Discussed in Thread: TPUL2T323

Tool/software:

Hi Experts,

My customer wants to check with us about the pulse duration time that SN74LVC1G123 output, can this duration time set to longer than 1 second with external RC setting?

Best Regards,

Remy

  • Hi Remy,

    Yes, you can using a large RC. However, if you are using a long pulse duration, I recommend looking at our new TPUL devices, such as the TPUL2T323. These devices are optimized for longer pulse widths and can achieve them using smaller RC components.

  • Hi Ian,

    Understood, for SN74LVC1G123, if we want to set Tout to 1 second, do we need to put a 100uF capacitor? Would this large RC brought us any potential problems?

    And for TPUL2T323, for 900ms pulse, it requires a 10uF cap, is there any method to replace this cap with a smaller cap? Such as 2.2uF cap. Customer still thinks 10uF cap is quite large in their design, resistor value can be higher.

    Best Regards,

    Remy

  • Hi Remy,

    For the SN74LVC1G123, you would need a large capacitor.

    For TPUL2T323, you can accomplish this with a 10 nF cap.