Part Number: SN74LVC1G126
Other Parts Discussed in Thread: UCC5350, , TMS320F28335, SN74LVC1G34
Hello E2E Experts,
Good day.
For my hardware experiment, I intend to use SN74LVC1G126 as buffer to interface the PWM coming from TMS320F28335 (µC) with UCC5350 (gate driver). The truth table as per the datasheet for the buffer is
|
OE |
A |
Y |
|
H |
H |
H |
|
H |
L |
L |
|
L |
X |
Z |
Looking at the buffer truth table, I personally don't feel there should be any issues. However, it wouldn't hurt if TI experts can give their opinion too.
The next question that I have is related to the routing of the buffer.
Can I route the decoupling capacitor between VCC and GND as has been done in the following image (taken from the datasheet of SN74LVC1G34, page 14):

Is the connecting trace running on the same layer directly below the IC? Can I do it for SN74LVC1G126 too?
Regards,
TICSC