Part Number: CD4504B
Other Parts Discussed in Thread: UCC27524, OPA4197, VFC110
Hello
I am trying to use this IC CD4504B for up-translating the 3.3 V Signals
of my MCU to +15V., using the Vcc as 5V, Vdd as 15 V and the Mode Select pin
to Vcc.
I get a proper functioning except at power-up, when I see a glitch
of sometimes 2V, sometimes over 10 V, lasting for a duration from a few mS to
to sometimes tens of mS.
Is this behaviour normal?
To overcome the Power-up timing of 5 & 15V, I put a Diode
With the anode to 5V and the cathode to the 15V pins, yet this glitch persists
Is this behaviour to be expected.
Thanks in advance