This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74ABT244A: Nexperia 74ABT244D Replacement

Part Number: SN74ABT244A

Hi Team,

Currently we found an opportunity to replace Nexperia 74ABT244D with TI SN74ABT244A. Customer needs a comparison table before input it in BOM. Could you please help provide it? I didn't find it on Seismic.

Thanks a lot.

BRs,

Francis 

  • Hi Francis,

    These devices are drop in replacements with no major differences. They were designed according to the same specs. The only difference between them is very slight differences in the typical propagation delay, but they have the same minimum and maximum values.

  • Hi Francis,

    Here is a comparison table for the devices. The TI is drop-in replacement. 

    Part Number SN74ABT244ADWR 74ABT244D, 623
    Supplier TI Nexperia
    Function 8-ch buffer with TTL-compatible CMOS inputs and 3-state outputs Octal buffer/line driver; 3-state
    Product Rating Catalog Catalog
    Logic Family ABT ABT
    Supply Voltage Range 4.5V - 5.5V 4.5V - 5.5V
    Logic Switching Levels TTL-Compatible CMOS TTL
    Output Type Push-pull Push-pull
    Output drive Strength - Min -32 mA -32 mA
    Output drive Strength - Max 64 mA 64 mA
    Operating temperature range (°C) -40 to 85 -40 to 85
    Package SOIC (12.8mm x 7.5mm) SOT163(12.8mm x 7.5mm)
    Over-voltage tolerant inputs? Yes Yes
    Equivalent Pinouts? Yes Yes
    Equivalent Packages? Yes Yes
    Pin2Pin solutions? Yes Yes

    Best Regards,

    Rajat Malani